Mail Icon postage letter Location Marker standard map marker Pencil Icon pencil Power Icon Lightning Bolt Radio Frequency Icon Radio Tower Radio Frequency Icon antenna Search Icon magnifying glass Outgoing Call Phone with arrow pointing out Incoming Call Phone with arrow pointing in Next Arrows 2 forward facing arrows Down Arrow Downward pointing arrow Download File tray with arrow pointing in Pencil pencil Document document Info info Power circle icon lightning bolt with circle around it RF Components circle icon antenna with circle around it Wolfspeed circle icon wolfspeed logo with circle around it Wolfspeed wolf icon wolfspeed logo Marker Icon with Circle map marker with circle Page Icon with Circle page marker with circle Gear Icon with Circle gear marker with circle Page Icon with Circle page marker with circle Play Button Triangle on top of circle Large Right Arrow Circle

Wolfspeed Delivers Industry’s First 1000V SiC MOSFET

10/6/2016

Durham, N.C., Oct. 6, 2016 – Wolfspeed, a Cree Company and a leader in silicon carbide (SiC) power products, has introduced a 1000V MOSFET that enables a reduction in overall system cost, while improving system efficiency and decreasing system-size. The new MOSFET, specially optimized for fast charging and industrial power supplies, enables a 30 percent reduction in component-count while achieving more than 3x increase in power density and a 33 percent increase in output power.

“Supporting the widespread implementation of off-board charging stations, Wolfspeed’s technology enables smaller, more efficient charging systems that provide higher power charging at lower overall cost. This market requires high efficiency and wide output voltage range to address the various electric vehicle battery voltages being introduced by automotive suppliers,” explained John Palmour, CTO of Wolfspeed.

“Wolfspeed’s new 1000V SiC MOSFET offers system designers ultra-fast switching speeds with a fraction of a silicon MOSFET’s switching losses. The figure-of-merit delivered by this device is beyond the reach of any competing silicon-based MOSFET,” Palmour added.

With the introduction of its 1000V SiC MOSFET, Wolfspeed leads the market with the industry’s most complete device portfolio. Wolfspeed was the first company to release a commercially qualified SiC MOSFET in 2011 and remains a leader today, committed to delivering great technology and value.

Designers can reduce component-count by moving from silicon-based, three-level topologies to simpler two-level topologies made possible by the 1000 Vds rating of the SiC MOSFET. The increase in output power in a reduced footprint is realized by the ultra-low output capacitance―as low as 60pF― which significantly lowers switching losses. This device enables operations at higher switching frequencies, which shrinks the size of the resonant tank elements and decreases overall losses, thus reducing heatsink requirements. Wolfspeed has determined these proof-points by constructing a 20kW full-bridge resonant LLC converter and comparing it to a market-leading 15kW silicon system.

Design Support

Wolfspeed offers a 20kW full-bridge resonant LLC converter reference design, listed as part number CRD-20DD09P-2. This fully assembled hardware set allows designers to quickly evaluate the new 1000V SiC MOSFET and demonstrate its faster switching capability—as well as the increased system power density the device enables.

The LLC converter's reference design files, which include full schematics, bill of materials, simulation files and detailed a user guide, can be found online at go.wolfspeed.com/referencedesigns. The full hardware is available for purchase on demand from Wolfspeed.
 

Device Information

The new 1000V, 65mOhm MOSFET is available in a through-hole, 4L-TO247 package and is listed as part number C3M0065100K and is currently available for purchase from several top distributors. Wolfspeed plans to release another 1000V MOSFET in a 4L-TO247 package at 120mOhm (C3M0120100K) in the coming weeks. This package has a Kelvin-source connection that allows engineers to create designs that maximize the benefits of SiC’s superior speed and efficiency.

The surface-mount versions of these devices, C3M0065100J and C3M0120100J, will be released later this year. Like the 4L-TO247, the surface mount devices include a Kelvin-source pin to help minimize gate-ringing and reduce system losses.

For more complete technical information about Wolfspeed’s new 1000V MOSFET, download its datasheet here. For all other inquiries about Wolfspeed power products, please visit http://www.wolfspeed.com/power/products

About Wolfspeed
Wolfspeed, A Cree Company, is leading the innovation and commercialization of silicon carbide and gallium nitride, liberating designers to invent power and wireless systems for a responsible, energy-efficient future.

Wolfspeed’s wide bandgap semiconductor products for power and radio-frequency (RF) applications deliver new levels of performance through increased efficiency, higher switching frequency and reduced system size and weight for the transportation, industrial, energy and communications markets.

Please refer to www.wolfspeed.com for additional product and company information.

About Cree
Cree is a market-leading innovator of lighting-class LEDs, lighting products and semiconductor products for power and radio frequency (RF) applications. Cree believes in better light experiences and is delivering new innovative LED technology that transforms the way people experience light through high-quality interior and exterior LED lighting solutions.

Cree’s product families include LED lighting systems and bulbs, blue and green LED chips, high-brightness LEDs, lighting-class power LEDs, power-switching devices and RF devices. Cree’s products are driving improvements in applications such as general illumination, electronic signs and signals, power supplies and inverters.

This press release contains forward-looking statements involving risks and uncertainties, both known and unknown, that may cause actual results to differ materially from those indicated. Actual results may differ materially due to a number of factors, including the risk that we may be unable to manufacture these new products with sufficiently low cost to offer them at competitive prices or with acceptable margins; the risk we may encounter delays or other difficulties in ramping up production of our new products; customer acceptance of our new products; the rapid development of new technology and competing products that may impair demand or render Cree’s products obsolete; and other factors discussed in Cree’s filings with the Securities and Exchange Commission, including its report on Form 10-K for the year ended June 26, 2016, and subsequent filings.

For additional product and Company information, please refer to www.cree.com.

Cree® is a registered trademark and Wolfspeed is a trademark of Cree, Inc.