Cree 231 Lumen Per Watt LED Shatters LED Efficacy Records
DURHAM, N.C. -- Cree, Inc. (Nasdaq: CREE), a market leader in LED lighting, reports another industry-best efficacy record of 231 lumens per watt for a white power LED. This result is a significant advance beyond Cree’s previous industry record and further demonstrates how Cree’s relentless innovation continues to push the boundaries of what is possible with LED lighting.
Cree reports that the LED efficacy was measured at 231 lumens per watt using a single-die component at a correlated color temperature of 4500 K. Standard room temperature 350 mA testing was used to achieve the results.
“It wasn’t long ago when 200 lumens per watt was considered the theoretical maximum efficiency for a lighting-class LED. We broke that barrier in 2010, and have now achieved 231 lumens per watt,” said John Edmond, Cree co-founder and director of advanced optoelectronics. “The innovation from our labs is the foundation for our industry-leading XLamp® LED family and an invention that continues our leadership of the LED lighting revolution.”
This R&D result features advanced aspects of the same technology used in Cree XLamp white LEDs. Cree believes higher-performance LEDs can enable new LED-based applications and drive down the solution cost of current LED-based designs.
While this level of performance is not yet available in Cree’s production LEDs, Cree continues to lead the industry with the broadest family of high-performance LEDs.
About Cree
Cree is leading the LED lighting revolution and making energy-wasting traditional lighting technologies obsolete through the use of energy-efficient, environmentally friendly LED lighting. Cree is a market-leading innovator of lighting-class LEDs, LED lighting, and semiconductor solutions for wireless and power applications.
Cree’s product families include LED fixtures and bulbs, blue and green LED chips, high-brightness LEDs, lighting-class power LEDs, power-switching devices and radio-frequency/wireless devices. Cree solutions are driving improvements in applications such as general illumination, backlighting, electronic signs and signals, variable-speed motors, and wireless communications.
For additional product and company information, please refer to www.cree.com. To learn more about the LED Lighting Revolution, please visit www.creeledrevolution.com.
This press release contains forward-looking statements involving risks and uncertainties, both known and unknown, that may cause actual results to differ materially from those indicated. Actual results may differ materially due to a number of factors, including the risk we may be unable to develop and release commercial products with performance comparable to the development results described above; the rapid development of new technology and competing products that may impair demand or render Cree's products obsolete; and other factors discussed in Cree's filings with the Securities and Exchange Commission, including its report on Form 10-K for the year ended June 27, 2010, and subsequent filings.