Cree Announces New GaN HEMT MMIC Power Amplifier
DURHAM, N.C. -- Cree, Inc. (Nasdaq: CREE) announces the release of a new GaN HEMT MMIC power amplifier, the CMPA0060025F, which offers 25 Watts output power over an instantaneous bandwidth of 20 MHz to 6 GHz. This product is ideal for military and ISM (industrial, scientific and medical) applications that require high power and broadband amplification up to 6GHz. The CMPA0060025F is packaged within a 0.25 square inch footprint, making it one of the smallest high-power amplifiers covering this bandwidth available in the marketplace. The MMIC can operate with supply voltages up to 50 volts and typically has 12 dB of power gain.
“The CMPA0060025F is a direct result of customer requests for a small, high-power, high-efficiency amplifier with performance through 6 GHz. It is designed to satisfy these requirements using Cree’s proven GaN MMIC foundry process and the convenient package format found in our other GaN MMIC products,” said Tom Dekker, Cree director of sales and marketing for RF Products. “We have received excellent customer feedback for our existing GaN MMIC products and are excited to be expanding this product line while continuing to offer custom MMIC foundry services.”
About Cree
Cree is a market-leading innovator of semiconductor solutions for wireless and power applications, lighting-class LEDs, and LED lighting solutions.
Cree’s product families include power-switching devices and radio-frequency/wireless devices, blue and green LED chips, high-brightness LEDs, lighting-class power LEDs, and LED fixtures and bulbs. Cree solutions are driving improvements in applications such as variable-speed motors, wireless communications, general illumination, backlighting and electronic signs and signals.
For additional product and company information, please refer to www.cree.com
This press release contains forward-looking statements involving risks and uncertainties, both known and unknown, that may cause actual results to differ materially from those indicated. Actual results may differ materially due to a number of factors, including the risk we may encounter delays or other difficulties in ramping up production of our new products; the potential lack of customer acceptance of the products; the rapid development of new technology and competing products that may impair demand or render Cree’s products obsolete; and other factors discussed in Cree’s filings with the Securities and Exchange Commission, including its report on Form 10-K for the year ended June 28, 2009, and subsequent filings.