Cree Announces New Generation of High-Power LEDs to Achieve Better Performance and Lowest System Cost
DURHAM, NC -- Cree, Inc. (Nasdaq: CREE) introduces the XLamp® MH-B LED, a new generation of high-power LEDs that delivers better performance and a more-effective way to achieve low-cost systems than mid-power (MP) LEDs. Using Cree’s high-reliability ceramic package technology, the XLamp MH-B LED is able to operate at higher temperatures than MP LEDs with no reduction in rated lifetime, enabling an impressive 60 percent reduction in heat-sink size and cost. Using up to 26 times fewer LEDs than MP LEDs to achieve the same level of performance, the XLamp MH-B is optimized to simplify LED system designs for applications where multiple MP LEDs are currently used.

“Cree has once again invented a lighting-optimized solution that can lower my costs and decrease manufacturing times,” said Frank Chen, technical director, Zhejiang Shenghui Lighting Co., Ltd. and Sengled Optoelectronics Co., Ltd. “While chip-on-board LEDs are an attractive alternative to MP LEDs in terms of reliability and cost, they aren’t compatible with my automated manufacturing processes. The new XLamp® MH-B LED finally gives me a more-reliable alternative to mid-power LEDs – I no longer have to compromise my brand and reputation to achieve a lower system cost.”
Featuring Cree’s EasyWhite® technology and a small 5-mm light-emitting surface, the XLamp MH-B provides many system benefits over arrays of MP LEDs, including tighter beam angles, simpler optics, a more-traditional appearance and easier color consistency. As a single LED, the XLamp MH-B LED delivers up to 830 lumens at 175 mA and can also be used in arrays to address higher-lumen applications that require low cost and high reliability, such as high bay, outdoor area and downlights.
“The new XLamp MH-B LED combines the reliability and manufacturability of Cree’s high power LEDs with the simplicity and performance of our CXA LED arrays,” said Paul Thieken, director of marketing, LED components. “MH-B introduces a new technology platform that gives customers the best of both technologies, while avoiding the limitations of mid-power LEDs.”
The XLamp MH-B LED is available in 2700 K – 6500 K with high-CRI options. Product samples are available now, and production quantities are available with standard lead times. Please visit www.cree.com/xlamp/mhb to learn more.
About Cree
Cree is leading the LED lighting revolution and making energy-wasting traditional lighting technologies obsolete through the use of energy-efficient, mercury-free LED lighting. Cree is a market-leading innovator of lighting-class LEDs, LED lighting, and semiconductor products for power and radio frequency (RF) applications.
Cree’s product families include LED fixtures and bulbs, blue and green LED chips, high-brightness LEDs, lighting-class power LEDs, power-switching devices and RF devices. Cree® products are driving improvements in applications such as general illumination, backlighting, electronic signs and signals, power suppliers and solar inverters.
Please refer to www.cree.com for additional product and company information.
This press release contains forward-looking statements involving risks and uncertainties, both known and unknown, that may cause actual results to differ materially from those indicated. Actual results may differ materially due to a number of factors, including the risk that actual savings will vary from expectations; the risk we may be unable to manufacture these new products with sufficiently low cost to offer them at competitive prices or with acceptable margins; the risk we may encounter delays or other difficulties in ramping up production of our new products; customer acceptance of LED products; the rapid development of new technology and competing products that may impair demand or render Cree’s products obsolete; and other factors discussed in Cree’s filings with the Securities and Exchange Commission, including its report on Form 10-K for the year ended June 29, 2014, and subsequent filings.