Cree Announces Sample Availability of Two New GaN HEMT Transistors
DURHAM, N.C. -- Cree, Inc. (Nasdaq: CREE) announces the sample release of two new GaN HEMT transistors, expanding the power range and addressable applications of the Cree product family.
The CGH40006P is a 6-watt GaN HEMT transistor covering a frequency range of DC through 6 GHz. This transistor is ideal for driver and medium power stages within broadband amplifier topologies. In addition, it can be used in low-noise amplifier applications where the superior ruggedness of GaN HEMTs can lessen the need for protection components, typically required in GaAs MESFET low-noise amplifiers.
A demonstration amplifier using the new transistor, at 28 volts operating voltage, provided a 2 to 6 GHz instantaneous bandwidth achieving 12 dB average small signal gain and 8 Watts typical saturated output power at greater than 50 percent drain efficiency over the entire band.
Cree has also introduced the CGH31240F, which is a high-power, class A/B S-Band GaN HEMT transistor. It is an internally-matched 240W packaged device for the 2.7 to 3.1 GHz band. It is designed for civil radar applications such as weather and air traffic control, as well as for marine radar. The CGH31240F, operating at 28V, offers over 10dB power gain while providing over 240 Watts saturated power with greater than 50 percent power added efficiency using a 300 microsecond, 10 percent duty cycle pulsed signal.
“The CGH40006P and CGH31240F are important new products which reflect our road map of GaN HEMT transistors and MMICs that offer higher power, bandwidth and ruggedness than conventional technologies such as GaAs and Si,” said Tom Dekker, Cree director of sales and marketing for RF Products.
About Cree
Cree is a market-leading innovator of semiconductor solutions for wireless and power applications, lighting-class LEDs, and LED lighting solutions.
Cree’s product families include power-switching devices and radio-frequency/wireless devices, blue and green LED chips, high-brightness LEDs, lighting-class power LEDs, and LED fixtures and bulbs. Cree solutions are driving improvements in applications such as variable-speed motors, wireless communications, general illumination, backlighting and electronic signs and signals.
For additional product and company information, please refer to www.cree.com
This press release contains forward-looking statements involving risks and uncertainties, both known and unknown, that may cause actual results to differ materially from those indicated. Actual results may differ materially due to a number of factors, including the risk we may encounter delays or other difficulties in ramping up production of our new sample products which are currently available for evaluation and testing purposes only; the risk we may be unable to develop and release commercial products with performance ratings comparable to the development results described above; the risk we may be unable to manufacture the products with sufficiently low cost to offer them at competitive prices or with acceptable margins; the potential lack of customer acceptance of the products; the rapid development of new technology and competing products that may impair demand or render Cree’s products obsolete; and other factors discussed in Cree’s filings with the Securities and Exchange Commission, including its report on Form 10-K for the year ended June 28, 2009, and subsequent filings.