LED Components
Cree Announces the Next Generation of High-Power XP-L LEDs
DURHAM, N.C. -- Cree, Inc. (Nasdaq: CREE) introduces the XLamp® XP-L2 LED, delivering up to seven percent more lumens and 15 percent higher lumens-per-watt (LPW) than the industry-leading XP-L LED. Leveraging elements of Cree’s breakthrough SC5 Technology™ Platform, the high-power XP-L2 LED improves the lumen density, voltage characteristics and reliability of the XP-L LED in the proven XP package. The new XP-L2 LED provides an easy drop-in upgrade to achieve higher system LPW for lighting manufacturers with existing XP-L designs, eliminating redesign costs. It also enables reduced size and cost for new designs.
“We like the XP-L2 LED because it is Cree innovation that we can leverage immediately,” said Nathan Heiking, product manager, Kenall Lighting. “The new XP-L2 LED improves upon the XP-L LED in the same footprint, allowing us to quickly achieve higher system efficacy in our existing XP designs without the burden of increased development time and cost.”
The XLamp XP-L2 LED raises efficacy of warm white (3000K, 80 CRI) at 85°C up to 171 LPW. In addition, the XP-L2 LED is now available in EasyWhite® 2-, 3- and 5-step color temperatures from 2700K to 6500K to enable luminaire color consistency. The XP-L2 LED has LM-80 data available immediately, enabling luminaires using XP-L2 to be qualified for ENERGY STAR® and DesignLights Consortium®.
“Cree created a breakthrough performance class of high-power LEDs with the XLamp® XP-L LED, and the new XP-L2 continues to strengthen our performance advantage,” said Dave Emerson, vice president and general manager for Cree LEDs. “The new XP-L2 LED delivers twice the lumen output of other similar-size high-power LEDs, enabling lighting manufacturers to improve the performance of their lighting designs and reduce the size and cost of new designs for applications, such as industrial and stadium lighting.”
Product samples are available now and production quantities are available with standard lead times. Please visit https://www.cree.com/xlamp/xpl2 to learn more.About Cree
Cree is a market-leading innovator of lighting-class LEDs, lighting products and semiconductor products for power and radio frequency (RF) applications. Cree believes in better light experiences and is delivering new innovative LED technology that transforms the way people experience light through high-quality interior and exterior LED lighting solutions.
Cree’s product families include LED lighting systems and bulbs, blue and green LED chips, high-brightness LEDs, lighting-class power LEDs, power-switching devices and RF devices. Cree’s products are driving improvements in applications such as general illumination, electronic signs and signals, power supplies and inverters.
Please refer to www.wolfspeed.com for additional product and Company information.
This press release contains forward-looking statements involving risks and uncertainties, both known and unknown, that may cause actual results to differ materially from those indicated. Actual results may differ materially due to a number of factors, including the risk that actual savings and lifetimes will vary from expectations; the risk we may be unable to manufacture these new products with sufficiently low cost to offer them at competitive prices or with acceptable margins; the risk we may encounter delays or other difficulties in ramping up production of our new products; customer acceptance of our new products; the rapid development of new technology and competing products that may impair demand or render Cree’s products obsolete; and other factors discussed in Cree’s filings with the Securities and Exchange Commission, including its report on Form 10-K for the year ended June 26, 2016, and subsequent filings.
Cree®, EasyWhite® and XLamp® are registered trademarks, and SC5 Technology™ is a trademark of Cree, Inc. ENERGY STAR® is a registered trademark of the U.S. Environmental Protection Agency. DesignLights Consortium® is a registered trademark of Northeast Energy Efficiency Partnerships, Inc.
# # #
More Articles
Jan 18, 2023
Wolfspeed, Inc. to Report Second Quarter Fiscal 2023 Earnings on January 25, 2023
Read More