Cree Increases Drive Current for XLamp® MX-6 Lighting-Class PLCC LED; Delivers 160% More Light Output
DURHAM, N.C. -- Cree, Inc. (Nasdaq: CREE), a market leader in LED lighting, announces a higher maximum forward drive current for the XLamp® MX-6 LED. The MX-6’s PLCC package is optimized for indoor lighting where enhanced light uniformity and LED-to-LED color consistency is important. At 1 A of current, XLamp MX-6 LEDs provide up to 300 lumens in cool white (6500 K) and 245 lumens in warm white (3000 K).
“At Lightfair 2010 in Las Vegas, Booth 746, we are relaunching our Raye fixture, which is now based on Cree MX-6 LEDs,” said Ann Reo, IO Lighting founder and general manager. “The MX-6 LED has dramatically reduced the power consumption for this cove and wall slot fixture, giving us superior luminaire efficacy. Raye is now a great retrofit option for existing fluorescent cove lighting applications because it delivers the same luminous intensity at 25 percent less power.”
“By qualifying our XLamp MX-6 LEDs at higher drive currents we are giving customers additional design flexibility,” said Paul Thieken, Cree director of marketing, LED Components. “Cree continues to ship the broadest portfolio of lighting-class LEDs, optimized for a wide range of lighting applications.”
About Cree
Cree is leading the LED lighting revolution and setting the stage to obsolete the incandescent light bulb through the use of energy-efficient, environmentally friendly LED lighting. Cree is a market-leading innovator of lighting-class LEDs, LED lighting, and semiconductor solutions for wireless and power applications.
Cree’s product families include LED fixtures and bulbs, blue and green LED chips, high-brightness LEDs, lighting-class power LEDs, power-switching devices and radio-frequency/wireless devices. Cree solutions are driving improvements in applications such as general illumination, backlighting, electronic signs and signals, variable-speed motors, and wireless communications.
For additional product and company information, please refer to www.cree.com. To learn more about the LED Lighting Revolution, please visit www.creeledrevolution.com.
This press release contains forward-looking statements involving risks and uncertainties, both known and unknown, that may cause actual results to differ materially from those indicated. Actual results may differ materially due to a number of factors, including customer acceptance of LED products; the rapid development of new technology and competing products that may impair demand or render Cree’s products obsolete; and other factors discussed in Cree’s filings with the Securities and Exchange Commission, including its report on Form 10-K for the year ended June 28, 2009, and subsequent filings.
Cree and XLamp are registered trademarks of Cree, Inc.