Cree Introduces Industry’s Brightest High-CRI LED Module
DURHAM, NC -- The new 6000-lumen LMH2 LED module from Cree (Nasdaq: CREE) is the industry’s brightest module to offer color-quality greater than 90 CRI at a consistent efficacy of 85 lumens per watt across a wide range of color temperatures (3000 K, 3500 K and 4000 K). The no-compromise LED solution is the ideal replacement for 100-watt ceramic-metal-halide lamps in high-ceiling applications, using 30 percent less power, lasting three times as long and delivering instant-on, dimmable light.

“The need for high-CRI and high-lumen-output LED luminaires has been growing rapidly over the last year. We constantly have requests for these luminaires to be used in shopping malls, airports, convention centers and theaters,” said Larry Rosenwinkel, fixtures and specifications manager, Facilities Solutions Group. “Before the introduction of the 6000-lumen Cree LMH2 LED module, there were no feasible LED solutions to light these spaces, but now we can specify LED light sources for these spaces.”
The Cree® LMH2 family of modules is the only light source that can address such a wide range of lighting applications in a common form factor. This allows lighting manufacturers to create an entire product portfolio with just one tooling set and one optical design. Lighting products based on the LMH2 LED module also enable lighting designers to illuminate a space with one light source and lighting technology, helping to eliminate the problems, such as color consistency and re-lamping, that come with using different lighting technologies.
“We have designs based on the 850-, 1250-, 2000-, 3000- and 4000-lumen LMH2 LED modules. The 6000-lumen LMH2 will allow us to further expand the breadth of our products using the same form factor,” said Wesley Johnson, director of national sales, Hi-Lite Manufacturing Company. “Our customers will now have a full suite of LED pendant lights and wall-mounted fixtures with the same high CRI, same color and same warranty that allows them to address a variety of ceiling-height applications.”
Lighting manufacturers looking to shorten the time-to-market for their luminaire design can also take advantage of the LMD600, Cree’s cost-effective, universal driver that is designed to power the new 6000-lumen LHM2. Dimmable to one percent, the LMD600 is optimized for a controllable, indoor architectural environment. The LMD600 can also handle up to 90°C case temperature and has a low-voltage, limited-energy-driver rating that does not require special enclosures or large-gauge wires, delivering design flexibility and a low system cost for lighting manufacturers. Cree also offers a range of reflectors and heat sinks, as well as a splice box for the entire LMH2 LED module family.
“Once again, Cree has demonstrated technology leadership by delivering 6000 lumens out of the same form factor in the LMH2 product line,” said Don Simmons, director of solid state lighting development, Pathway Lighting, Inc. “The new and brighter 6000-lumen LMH2 LED module will allow us to replace 100-watt ceramic-metal-halide solutions and address high-ceiling applications.”
The complete LMH2 module family is available in a range of lumens (850 to 6000) and color temperatures (2700 K to 4000 K), delivering up to 108 lumens-per-watt efficacy and a CRI greater than 90. These lighting characteristics combined with multiple driver options, including digital-addressable lighting interface (DALI) and DALI® touch-dimming driver options, enable lighting manufacturers to expand their portfolio quickly and easily. Designed for 50,000 hours of operation, the LMH2 module comes with Cree’s industry-leading five-year warranty. The LMH2 is also UL-recognized and complies with multiple international regulatory and safety standards. Luminaire makers seeking ENERGY STAR® qualification will have access to specification and performance data, including LM-80 reports, which can speed regulatory approvals.
Samples and production quantities are available with standard lead times from Cree distributors. Please visit www.cree.com/lmh2 for additional information.
About Cree
Cree is leading the LED lighting revolution and making energy-wasting traditional lighting technologies obsolete through the use of energy-efficient, mercury-free LED lighting. Cree is a market-leading innovator of lighting-class LEDs, LED lighting, and semiconductor products for power and radio frequency (RF) applications.
Cree’s product families include LED fixtures and bulbs, blue and green LED chips, high-brightness LEDs, lighting-class power LEDs, power-switching devices and RF devices. Cree® products are driving improvements in applications such as general illumination, backlighting, electronic signs and signals, power suppliers and solar inverters.
For additional product and company information, please refer to www.cree.com.
This press release contains forward-looking statements involving risks and uncertainties, both known and unknown, that may cause actual results to differ materially from those indicated. Actual results may differ materially due to a number of factors, including the risk that actual savings and lifetimes will vary from expectations; the risk we may be unable to manufacture these new products with sufficiently low cost to offer them at competitive prices or with acceptable margins; the risk we may encounter delays or other difficulties in ramping up production of our new products; customer acceptance of LED products; the rapid development of new technology and competing products that may impair demand or render Cree’s products obsolete; and other factors discussed in Cree’s filings with the Securities and Exchange Commission, including its report on Form 10-K for the year ended June 30, 2013, and subsequent filings.
Cree® is a registered trademark of Cree, Inc.
DALI® is a registered trademark of ZVEI-Zentralverband Elektrotechnik- und Elektronikindustrie e.V.
ENERGY STAR® is a registered trademark of the U.S. Environmental Protection Agency.