Cree LMH2 Module Delivers Industry’s First No-Compromise Sunset Dimming Experience
DURHAM, NC -- Cree, Inc. (Nasdaq: CREE) introduces the LMH2 LED Module with sunset dimming – Cree’s game-changing dimming technology that provides a dimming experience similar to incandescent lighting. The new module enables a natural dimming profile that was previously unachievable with any other energy-saving technology. Cree’s sunset dimming technology dims smoothly from 2700 K to 1800 K, delivering rich, warm light for applications requiring a traditional style of dimming, such as hospitality and residential settings, while still achieving over 80-percent energy reduction compared to energy-inefficient incandescents.

The robust LMH2 module family now lets lighting manufacturers address a wide range of lighting technologies with a one module form factor. The aesthetically pleasing module leverages one product platform to create an entire luminaire portfolio — delivering the investment protection necessary to quickly and cost effectively address most lighting applications.
“The Cree® LMH2 LED module enables us to address a wide range of lighting applications with a single platform, providing investment protection,” said Kenny Eidsvold, president, Intense Lighting, Inc. “We recently launched a new product line based on the 4000-lumen LMH2 LED module. Now with the introduction of Cree’s sunset-dimming option, we can further expand our product line to offer quality LED lighting solutions for hospitality, restaurant and residential applications.”
Available in a range of lumens (850 to 3000) at 2700 K and multiple driver options, LMH2 modules with sunset-dimming technology can plug in seamlessly to existing LMH2 module drivers and reflectors, and are also compatible with TRIAC dimmers — meaning the high-performance module can be easily retrofitted in any room with traditional dimming technologies or used in new installations with 0–10 V or digital addressable lighting interface (DALI) dimming technologies.
“Cree’s LMH2 sunset dimming is the best implementation of sunset dimming that we have found on the market today,” said Fred Farzan, president of Nora Lighting. “Our customers really like the color quality and natural dimming the LMH2 sunset dimming provides. The LMH2 module with sunset dimming opens up new markets for us and allows us to address applications that traditionally use incandescent and halogen light sources.”
“We really like Cree LMH2’s implementation of sunset dimming,” said Mike Wang, vice president, lighting engineering, Edison Price Lighting. “The LMH2 LED module delivers rich, warm light while maintaining high CRI to provide the look and feel of a traditional incandescent lamp.”
Designed for 50,000 hours of operation and dimmable to five percent, the LMH2 module comes with Cree’s industry-leading, five-year warranty. Luminaire makers seeking ENERGY STAR® qualification will have access to specification and performance data, including LM-80 reports, which can speed regulatory approvals.
Cree LMH2 LED Modules with sunset dimming samples are available now. Production quantities are available with standard lead times. Please visit www.cree.com/modules to learn more.
About Cree
Cree is leading the LED lighting revolution and making energy-wasting traditional lighting technologies obsolete through the use of energy-efficient, mercury-free LED lighting. Cree is a market-leading innovator of lighting-class LEDs, LED lighting, and semiconductor products for power and radio frequency (RF) applications.
Cree’s product families include LED fixtures and bulbs, blue and green LED chips, high-brightness LEDs, lighting-class power LEDs, power-switching devices and RF devices. Cree® products are driving improvements in applications such as general illumination, backlighting, electronic signs and signals, power suppliers and solar inverters.
For additional product and company information, please refer to www.cree.com.
This press release contains forward-looking statements involving risks and uncertainties, both known and unknown, that may cause actual results to differ materially from those indicated. Actual results may differ materially due to a number of factors, including the risk that actual savings and lifetimes will vary from expectations; the risk we may be unable to manufacture these new products with sufficiently low cost to offer them at competitive prices or with acceptable margins; the risk we may encounter delays or other difficulties in ramping up production of our new products; customer acceptance of LED products; the rapid development of new technology and competing products that may impair demand or render Cree’s products obsolete; and other factors discussed in Cree’s filings with the Securities and Exchange Commission, including its report on Form 10-K for the year ended June 30, 2013, and subsequent filings.
Cree® is a registered trademark of Cree, Inc.
ENERGY STAR® is a registered trademark of the U.S. Environmental Protection Agency.