Cree’s New XLamp MHD Family Delivers Chip-on-Board Performance in a Surface-Mount LED
DURHAM, NC -- Building on the success of the groundbreaking XLamp® MH family of LEDs, Cree, Inc. (Nasdaq: CREE) introduces the XLamp MHD-E and MHD-G LEDs, the high-power LEDs that combine the high lumen density and reliability of a ceramic chip-on-board LED with the design and manufacturing advantages of a surface-mount package. Utilizing elements of the Cree SC5 Technology™ Platform, the ceramic XLamp MHD LEDs simplify development, increase design flexibility and improve manufacturing efficiency compared to mid-power LEDs. The MH family enables new designs and significantly lower system costs, all while delivering industry-leading performance.
“The high lumen output and high reliability of Cree’s new MHD-G LED allows us to develop a new downlight that outperforms other downlights in the market,” said Baly Luo, general manager, Aeon Lighting Technology. “ALT’s compact-size, 4-inch downlight that is built with the MHD-G LED generates over 1,800 lumens at 3000 K while other downlights can only produce 800 to 1000 lumens.”

Featuring Cree EasyWhite® technology in a 7-mm x 7-mm package, XLamp MH LEDs enable a smaller board size, tighter beam angle and a more traditional appearance than mid-power LEDs. Delivering more than 1800 lumens at 14 W and 2500 lumens at 19 W respectively, the XLamp MHD-E and MHD-G LEDs are ideal for semi-directional, high-lumen applications such as downlights, high-bay and outdoor area applications.
“At Cree, we continue to deliver innovative products that give our customers a competitive edge in the marketplace,” said Paul Thieken, Cree director of marketing, LED Components. “With the MHD LEDs, we’re offering chip-on-board performance to lighting manufacturers that prefer surface-mount technology, making it easier for them to achieve lower system cost than with the same commoditized mid-power LEDs that everyone is using.”
Cree XLamp MHD-E and MHD-G LEDs are available in 2700 K – 6500 K with high-CRI and multiple voltage options. Product samples are available now, and production quantities are available with standard lead times. Please visit www.cree.com/xlamp/mh to learn more.
About Cree
Cree is leading the LED lighting revolution and making energy-wasting traditional lighting technologies obsolete through the use of energy-efficient, mercury-free LED lighting. Cree is a market-leading innovator of lighting-class LEDs, LED lighting, and semiconductor products for power and radio frequency (RF) applications.
Cree’s product families include LED fixtures and bulbs, blue and green LED chips, high-brightness LEDs, lighting-class power LEDs, power-switching devices and RF devices. Cree® products are driving improvements in applications such as general illumination, backlighting, electronic signs and signals, power suppliers and solar inverters.
Please refer to www.cree.com for additional product and company information.
This press release contains forward-looking statements involving risks and uncertainties, both known and unknown, that may cause actual results to differ materially from those indicated. Actual results may differ materially due to a number of factors, including the risk that actual savings and lifetimes will vary from expectations; the risk we may be unable to manufacture these new products with sufficiently low cost to offer them at competitive prices or with acceptable margins; the risk we may encounter delays or other difficulties in ramping up production of our new products; customer acceptance of new LED products; the rapid development of new technology and competing products that may impair demand or render Cree’s products obsolete; and other factors discussed in Cree’s filings with the Securities and Exchange Commission, including its report on Form 10-K for the year ended June 29, 2014, and subsequent filings.
Cree®, EasyWhite® and XLamp® are registered trademarks, and SC5 Technology™ is a trademark of Cree, Inc.