Cree Introduces Highest Power & Frequency Packaged GaN HEMT
DURHAM, NC -- Cree, Inc. (Nasdaq: CREE) introduces the industry’s highest power continuous wave (CW) GaN HEMT RF transistors packaged in a dual-flat no-leads (DFN) format. Aimed at the cost-sensitive sub-100W commercial radar and data link amplifier market segments, the new 6- and 25-watt DFN transistors effectively obsolete the use of inefficient GaAs transistors in C- and X-Band frequencies and also enable the practical replacement of short life tube-based technology for commercial radar applications such as weather, marine and surveillance.
Based on Cree’s proven 40V, 0.25 µm gate length high frequency process, Cree® GaN DFN transistors deliver twice the PSAT efficiency and transistor gain of GaAs IMFETs in a package size that is nearly 20 times smaller at comparable power levels and frequencies. In high capacity microwave data links used in enterprise, point-to-point and airborne communication networks, the new transistors extend the communication range while delivering twice the linear efficiency of GaAs-based amplifiers. This higher efficiency gives RF designers the flexibility needed to reduce amplifier size and weight, creating tremendous savings in operating and total lifecycle costs.
“For years, commercial microwave radar transmitters have been plagued with the compromised field life of tube-based amplifiers that carry significant maintenance costs. Historically, high capacity data links were limited to the use of inefficient GaAs IMFETs,” said Tom Dekker, director of RF sales and marketing, Cree, Inc. “By delivering superior efficiency and power capabilities at an affordable price, our new GaN DFN transistors enable for the first time the replacement of these legacy technologies in lower power, cost-sensitive commercial systems.”
The new DFN devices also make excellent drivers for Cree’s popularCGHV96100 and CGHV96050F2 fully-matched FETs for X-Band, enabling the output and drive stage transistors to operate from the same voltage rail. This allows convenient, regulated power distribution to economize board space compared with a mixed voltage transistor line up.
Samples and reference designs for C- and X-Band are available now utilizing the CGHV1F006S (6W) and CGHV1F025S (25W) GaN DFN transistors. Large signal models are also available for Agilent’s ADS and AWR Microwave Office simulators.
About Cree
Cree is a market-leading innovator of semiconductor products for power and radio-frequency (RF) applications, lighting-class LEDs and LED lighting solutions.
Cree's product families include LED fixtures and bulbs, blue and green LED chips, high-brightness LEDs, lighting-class power LEDs, power-switching devices and RF devices. Cree products are driving improvements in applications such as general illumination, electronic signs and signals, power supplies and solar inverters.
Please refer to www.cree.com for additional product and company information.
This press release contains forward-looking statements involving risks and uncertainties, both known and unknown, that may cause actual results to differ materially from those indicated. Actual results may differ materially due to a number of factors, including the risk that actual savings will vary from expectations; the risk we may be unable to manufacture these new products with sufficiently low cost to offer them at competitive prices or with acceptable margins; the risk we may encounter delays or other difficulties in ramping up production of our new products; customer acceptance of our new products; the rapid development of new technology and competing products that may impair demand or render Cree’s products obsolete; and other factors discussed in Cree’s filings with the Securities and Exchange Commission, including its report on Form 10-K for the year ended June 30, 2013, and subsequent filings.