New High-Efficiency Cree XLamp® LED Can Reduce Initial Fixture Cost for Lighting Manufacturers
DURHAM, N.C. -- Cree, Inc. (Nasdaq: CREE), a market leader in LED lighting, announces the commercial availability of XLamp® XP-E High Efficiency White (HEW) LEDs. The new high-efficiency components extend the light output and efficacy of the award-winning XLamp XP-E LED family, enabling fixture designs that can use up to 50 percent fewer LEDs, which can help drive down costs for fixture and bulb manufacturers while delivering the same system performance.
XP-E HEW LEDs are optimized to lower initial costs for diffuse lighting applications, such as LED replacement lamps and downlights. For example, an A-19 lamp that uses XP-E LEDs could be re-designed to use half as many XP-E HEW LEDs while maintaining the same efficacy.
“One of the major barriers to LED lighting adoption and design remains upfront cost,” said Paul Thieken, Cree director of marketing, LED components. “By enabling designers to use brighter, precisely-optimized LEDs for each particular application, Cree is helping lower costs and further simplifying and shortening the LED fixture design cycle.”
XLamp XP-E High Efficiency White LEDs are the first high-power LEDs featuring Cree’s new Direct Attach™ LED technology. Direct Attach technology is Cree’s unique, next-generation LED chip technology that delivers higher flux, lower forward voltage, and lower thermal resistance.
“With 500 percent more die-attach area and an order-of-magnitude less die under-fill, Direct Attach technology is far more robust than any other LED flip chip technology in the market today,” said John Edmond, Cree director of advanced optoelectronics. “For our customers, these attributes, combined with the performance advantages of Direct Attach technology, can translate to brighter, more reliable lamps and fixtures, developed at a lower cost.”
XLamp XP-E High Efficiency White LEDs deliver up to 148 lumens in cool white (6500K) and 114 lumens in warm white (3000K) at 350 mA. In addition to light output and efficacy improvements, XP-E HEW LEDs feature a reduced thermal resistance of 6 °C/W. XP-E HEW LEDs are available in the same white variations as XP-E LEDs, including Standard White, Outdoor White and 80-CRI White.
XLamp XP-E High Efficiency White LEDs are available now in sample and production quantities with standard lead times. IES LM-80 data for measuring lumen maintenance of LED light sources, for XP-E HEW LEDs, is targeted for availability in February 2011. To locate a distributor, please visit www.cree.com
About Cree
Cree is leading the LED lighting revolution and making energy-wasting traditional lighting technologies obsolete through the use of energy-efficient, environmentally friendly LED lighting. Cree is a market-leading innovator of lighting-class LEDs, LED lighting, and semiconductor solutions for wireless and power applications.
Cree’s product families include LED fixtures and bulbs, blue and green LED chips, high-brightness LEDs, lighting-class power LEDs, power-switching devices and radio-frequency/wireless devices. Cree solutions are driving improvements in applications such as general illumination, backlighting, electronic signs and signals, variable-speed motors, and wireless communications.
For additional product and company information, please refer to www.cree.com. To learn more about the LED Lighting Revolution, please visit www.creeledrevolution.com.
This press release contains forward-looking statements involving risks and uncertainties, both known and unknown, that may cause actual results to differ materially from those indicated. Actual results may differ materially due to a number of factors, including the risk we may encounter delays or other difficulties in ramping up production of our new products; the rapid development of new technology and competing products that may impair demand or render Cree’s products obsolete; and other factors discussed in Cree’s filings with the Securities and Exchange Commission, including its report on Form 10-K for the year ended June 27, 2010, and subsequent filings.