Mail Icon postage letter Location Marker standard map marker Pencil Icon pencil Power Icon Lightning Bolt Radio Frequency Icon Radio Tower Radio Frequency Icon antenna Search Icon magnifying glass Outgoing Call Phone with arrow pointing out Incoming Call Phone with arrow pointing in Next Arrows 2 forward facing arrows Down Arrow Downward pointing arrow Download File tray with arrow pointing in Pencil pencil Document document Info info Power circle icon lightning bolt with circle around it RF Components circle icon antenna with circle around it Wolfspeed circle icon wolfspeed logo with circle around it Wolfspeed wolf icon wolfspeed logo Marker Icon with Circle map marker with circle Page Icon with Circle page marker with circle Gear Icon with Circle gear marker with circle Page Icon with Circle page marker with circle Play Button Triangle on top of circle Large Right Arrow Circle Facebook Icon Twitter logo LinkedIn logo YouTube logo Right Arrow Right Arrow - thinner Handshake Icon Envelope Icon

Cree Announces Low Cost Extended Bandwidth GaN HEMT Transistors

5/7/2014

DURHAM, NC -- As high data rate applications put more strain on LTE wireless networks, innovative solutions such as small cell base stations (BTS) and carrier aggregation will be needed to bridge the bandwidth gap in high traffic areas. In response to broader bandwidth demand, Cree, Inc. (Nasdaq: CREE) introduces a family of GaN HEMT RF transistors that delivers industry-leading bandwidth and high efficiency performance to support today’s busy LTE networks. Built on plastic dual-flat no-leads (DFN) surface mount packages, the new Cree® GaN HEMT RF transistors also provide the affordability needed to replace less efficient Si or GaAs transistors in these applications.

“The trend of ever-increasing amounts of data-rich applications will drive the need for small cell deployment to improve wireless network performance,” said Tom Dekker, director of sales and marketing, RF Business Unit, Cree, Inc. “Our industry-leading GaN technology will provide the desired bandwidth, flexibility, efficiency and affordability our small cell customers demand.”

The new GaN HEMT DFN product family includes 28V and 50V, 15W and 30W unmatched transistors. The frequency-agile transistors are capable of operating at a range between 700 MHz to 3.8 GHz instantaneous, and may be optimized for band splits. Multi-band capability creates design flexibility that helps small cell OEMs speed their time to market and allows operators to reconfigure the same small cell unit for different market requirements. 

In high efficiency applications, Cree GaN HEMT RF transistors help reduce the size and weight of LTE cellular network transmitters and simplify thermal management. These efficiency gains generate significant energy savings in operational costs. Cree developed Doherty reference design CDPA27045 utilizing 15W and 30W HEMT DFN transistors to demonstrate the technology’s superior efficiency. The design delivers approximately 50 percent drain efficiency at 10W average power under a LTE 7.5dB peak-to-average ratio signal, and covers 2.5-2.7 GHz instantaneous RF bandwidth while offering 16dB of linear gain.

The new family of GaN HEMT DFN RF transistors is based on Cree’s qualified 50V, 0.4µm gate length process. Samples and reference designs are available for the CGH27030S (30W, 28V, 0.4µm), CGHV27015S (15W, 50V, 0.4µm) and CGHV27030S (30W, 50V, 0.4µm) GaN HEMT transistors. 

Visit www.cree.com/smallcell for more information.

About Cree
Cree is a market-leading innovator of semiconductor products for power and radio-frequency (RF) applications, lighting-class LEDs and LED lighting solutions. 

Cree's product families include LED fixtures and bulbs, blue and green LED chips, high-brightness LEDs, lighting-class power LEDs, power-switching devices and RF devices. Cree products are driving improvements in applications such as general illumination, electronic signs and signals, power supplies and solar inverters.

Please refer to www.cree.com for additional product and company information.

This press release contains forward-looking statements involving risks and uncertainties, both known and unknown, that may cause actual results to differ materially from those indicated. Actual results may differ materially due to a number of factors, including the risk that actual savings will vary from expectations; the risk we may be unable to manufacture these new products with sufficiently low cost to offer them at competitive prices or with acceptable margins; the risk we may encounter delays or other difficulties in ramping up production of our new products; customer acceptance of our new products; the rapid development of new technology and competing products that may impair demand or render Cree’s products obsolete; and other factors discussed in Cree’s filings with the Securities and Exchange Commission, including its report on Form 10-K for the year ended June 30, 2013, and subsequent filings.