What industries and applications can benefit from Wolfspeed WolfPACK™ modules?
Article
As part of its ongoing commitment to designing silicon carbide (SiC) components which power today’s technology solutions, Wolfspeed has announced the launch of its new line of Wolfspeed WolfPACK™ power modules. This new product family is meant to serve today’s designers with a mid-power solution across a wide range of application types.
The Wolfspeed WolfPACK modules are easy to scale and provide higher ampacity as compared to the same topology with multiple discreet devices. These modules are available in half-bridge, full-bridge, and six-pack (three-phase) configurations, all with the option of pre-applied thermal interface material (TIM).
The Wolfspeed WolfPACK power module line supports a diverse range of applications. Let’s explore a few in more detail:
Car charging stations
The demand for electric vehicles (EVs) has increased considerably in recent years, but one key area that will lead to tangible, rapid growth is the ability to provide fast chargers. One of the biggest advantages of fossil fuel vehicles over electric vehicles is the former’s ability to be refuelled in minutes. EVs on the other hand can take much longer to be ready to return to the road; different charging designs can take as little as 30 minutes to charge or as much as twelve hours1. Fast charging technology can shorten the recharging time by transferring large amounts of energy quickly using higher voltages, higher currents, or a combination of both.
Wolfspeed WolfPACK power modules’ SiC technology and their high ampacity capabilities make them ideal for fast-charging environments. The small profile of these modules allows for use in many different locations, whether it’s large gas stations or space-constrained urban recharging locations. Furthermore, the modules’ scalability allows manufacturers to develop scalable charging systems, a consideration that will become increasingly important as the energy capacities of EVs increase.
Renewable energy
To support a more sustainable energy future, reduced reliance on fossil fuels is also required in the energy sector — which requires a rise in renewable energy solutions, such as wind and solar. While these power sources are environmentally friendly, both produce electricity that cannot be directly fed into the grid — thus they require additional power conversion steps to be viable.
The power generated by wind turbines may require an AC/DC converter, which is used to convert AC power (which will not be synced to the grid’s frequency or phase) into DC power. When that’s complete, the power is then converted back into AC for use with the grid. Solar panels, meanwhile, produce DC power only, and so require an inverter if they are to be connected to the grid.
Depending on the deployment, power distribution systems for renewable energy may be size-constrained, which is the case for residential-based solar installations that are often mounted to utility poles. The SiC MOSFET technology featured in the Wolfspeed WolfPACK modules allows for overall reduced size of power conversion systems through an increase in power density. When reviewing the system level savings associated with a shift to silicon carbide, photovoltaic (PV) inverters have been demonstrated to reduce size, weight, and cost from 20 to 50% when compared to Si-based technology, while maintaining or even increasing efficiency2. This is due to the optimal material properties of silicon carbide; the wider bandgap enables higher breakdown voltage and higher junction temperature operation, resulting in higher power density than Si with higher efficiency. Any increase in efficiency is critical to supporting a better power distribution network, as it results in less lost energy — just a 1% increase in efficiency would equate to an additional 600 megawatts of solar power annually from the 60 gigawatts of solar installed in the United States3. If you’re curious about how to frame the energy savings from this efficiency increase, the Department of Energy published a series on how much to put just 1 gigawatt, which is 1 billion watts, into perspective.
Energy storage
An increase in renewable energy not only requires power conversion for viability, but also requires that power is available to meet consumer and industrial demand at all hours, every day of the year. In some cases, renewable energy sources under-produce due to sub-optimal ambient conditions, while other times they can create excessive energy above immediate demand. To resolve this discrepancy between stable energy supply and demand, large-scale energy storage systems, such as batteries, are implemented. These systems charge during high renewable energy generation periods and discharge back to the grid when renewable energies cannot meet peak energy demands.
As with the power conversion requirements of renewable energy, Wolfspeed WolfPACK SiC modules are ideal for renewable energy storage solutions due to the inherent increases in system density and efficiency associated with silicon carbide technology. This modules’ ability to create easily scalable solutions, coupled with its reduced size footprint, makes the technology ideal for developing renewable energy infrastructure supporting grid-supply to meet demand.
Industrial Power Systems
Industrial power systems apply across several types of industrial sectors: from data centers to airports, manufacturing to automotive, and more. While many industrial power systems are built with a focus on expandability, automation, and adaptability, these systems also demand reliability — as downtime of any piece of equipment can become costly. In such industrial applications, reliability is the most crucial element of decision making because downtime means huge.
Wolfspeed WolfPACK modules are ideal for industrial power systems, thanks to the company’s proven trillion-hour record that demonstrates field reliability. The low inductance and low switching losses of these modules make them ideal for high-frequency operation in applications including motor control systems, power converters, and welders. Furthermore, the modules feature baseplate-less packaging which, when coupled with the company’s leading SiC technology solutions, affords system designers flexible thermal management implementation.
Conclusion
Wolfspeed WolfPACK modules offer tremendous potential across a range of industries and applications, including EV charging, renewable energy, energy storage, and industrial power systems, among others. Its ease of implementation, coupled with the high efficiency and superior performance of silicon carbide package for medium power range solutions.
Learn more about Wolfspeed WolfPACK™ power modules.
Featured Products
Wolfspeed WolfPACK™ Silicon Carbide Power Modules Family
Wolfspeed WolfPACK™ Silicon Carbide Power Modules Family
Wolfspeed WolfPACK™ Silicon Carbide Power Modules Family
Product SKU | Buy Online | Request Sample | Data Sheet | Package | Configuration | Blocking Voltage | Current Rating | RDS(ON) at 25°C | Generation | Maximum Junction Temperature | Module Size |
---|---|---|---|---|---|---|---|---|---|---|---|
GM3 | Half-Bridge | 1200 V | 200 A | 6 mΩ | Gen 3 MOS | 150 °C | 62.8 mm x 56.7 mm | ||||
GM3 | Half Bridge (AlN substrate) | 1200 V | 200 A | 6 mΩ | Gen 3 MOS | 150 °C | 62.8 mm x 56.7 mm | ||||
GM3 | Half-Bridge | 1200 V | 200 A | 6 mΩ | Gen 3 MOS | 150 °C | 62.8 mm x 56.7 mm | ||||
GM3 | Half Bridge (AlN substrate) | 1200 V | 200 A | 6 mΩ | Gen 3 MOS | 150 °C | 62.8 mm x 56.7 mm | ||||
GM3 | Half Bridge (AlN substrate) | 1200 V | 181 A | 8 mΩ | Gen 3 MOS | 150 °C | 62.8 mm x 56.7 mm | ||||
GM3 | Half-Bridge | 1200 V | 160 A | 8 mΩ | Gen 3 MOS | 150 °C | 62.8 mm x 56.7 mm | ||||
GM3 | Half-Bridge | 1200 V | 160 A | 8 mΩ | Gen 3 MOS | 150 °C | 62.8 mm x 56.7 mm | ||||
GM3 | Half Bridge (AlN substrate) | 1200 V | 181 A | 8 mΩ | Gen 3 MOS | 150 °C | 62.8 mm x 56.7 mm | ||||
FM3 | Half-Bridge | 1200 V | 117 A | 11 mΩ | Gen 3 MOS | 150 °C | 62.8 mm x 33.8 mm | ||||
FM3 | Half-Bridge | 1200 V | 117 A | 11 mΩ | Gen 3 MOS | 150 °C | 62.8 mm x 33.8 mm | ||||
GM3 | Half-Bridge | 1200 V | 141 A | 11 mΩ | Gen 3 MOS | 150 °C | 62.8 mm x 56.7 mm | ||||
GM3 | Half-Bridge | 1200 V | 141 A | 11 mΩ | Gen 3 MOS | 150 °C | 62.8 mm x 56.7 mm | ||||
FM3 | Half-Bridge | 1200 V | 84 A | 16 mΩ | Gen 3 MOS | 150 °C | 62.8 mm x 33.8 mm | ||||
FM3 | Half-Bridge | 1200 V | 84 A | 16 mΩ | Gen 3 MOS | 150 °C | 62.8 mm x 33.8 mm | ||||
GM3 | Six-pack (three-phase) | 1200 V | 50 A | 16 mΩ | Gen 3 MOS | 150 °C | 62.8 mm x 56.7 mm | ||||
GM3 | Six-pack (three-phase) | 1200 V | 50 A | 16 mΩ | Gen 3 MOS | 150 °C | 62.8 mm x 56.7 mm | ||||
FM3 | Six-pack (three-phase) | 1200 V | 30 A | 21 mΩ | Gen 3 MOS | 150 °C | 62.8 mm x 33.8 mm | ||||
FM3 | Full-Bridge | 1200 V | 48 A | 21 mΩ | Gen 3 MOS | 150 °C | 62.8 mm x 33.8 mm | ||||
FM3 | Six-pack (three-phase) | 1200 V | 30 A | 21 mΩ | Gen 3 | 150 °C | 62.8 mm x 33.8 mm | ||||
FM3 | Full-Bridge | 1200 V | 48 A | 21 mΩ | Gen 3 MOS | 150 °C | 62.8 mm x 33.8 mm | ||||
FM3 | Six-pack (three-phase) | 1200 V | 30 A | 32 mΩ | Gen 3 MOS | 150 °C | 62.8 mm x 33.8 mm | ||||
FM3 | Full-Bridge | 1200 V | 37 A | 32 mΩ | Gen 3 MOS | 150 °C | 62.8 mm x 33.8 mm | ||||
FM3 | Six-pack (three-phase) | 1200 V | 30 A | 32 mΩ | Gen 3 MOS | 150 °C | 62.8 mm x 33.8 mm | ||||
FM3 | Full-Bridge | 1200 V | 37 A | 32 mΩ | Gen 3 MOS | 150 °C | 62.8 mm x 33.8 mm |
Featured Design Tools
We lead the pack by making sure silicon carbide system education and design resources are right at your fingertips through our reference designs, evaluation kits, gate drivers, and technical resources. Learn more about Wolfspeed WolfPACK companion parts to better understand how this new module platform can help you increase product performance, accelerate time to market, and lower costs.
Products
Products
Name | Buy Online | Form | Package | Designed By | Product SKU | View Product |
---|---|---|---|---|---|---|
Evaluation Tool | FM3 | Wolfspeed | KIT-CRD-CIL12N-FMA | |||
Evaluation Tool | FM3 | Wolfspeed | KIT-CRD-CIL12N-FMC | |||
Evaluation Tool | GM3 | Wolfspeed | KIT-CRD-CIL12N-GMA | |||
Gate Driver Board | FM3, GM3, SpeedVal Kit | Skyworks | ||||
Gate Driver Board | FM3, GM3, SpeedVal Kit | Analog Devices | ||||
Gate Driver Board | FM3, GM3, SpeedVal Kit | Wolfspeed | CGD1700HB2M-UNA |