Skip to Main Content
Contact
  • English
  • 简体中文
  • 繁體中文
View Cart
SiC Materials

Materials Products

Wolfspeed is transitioning to a new wafer scribe format based upon SEMI specification M12-0706. This conversion is projected to be fully integrated across all products by the end of 2023, and brings several improvements. The M12-based scribe will be positioned upright when the major flat or notch is oriented up, making the scribe easier to read when the wafers are loaded into cassettes. The new format includes a wafer supplier identification code, validating the wafer’s authenticity. It also includes a checksum, which is an error-detection method that prevents OCR mis-read errors and reduces the instance of processing errors associated with such event.

Industry-Leading Portfolio, Innovation and Scale

With more than 30 years of SiC development and manufacturing experience, Wolfspeed produces the industry’s broadest range of SiC materials. Offering n-type conductive SiC products and a variety of SiC epitaxy options, Wolfspeed delivers the quality and quantity necessary to support the rapidly expanding demand for high-efficiency, SiC power semiconductors.

When you partner with Wolfspeed, you get the best and most innovative materials.


Products

N-Type
SiC Substrates
HPSI
Semi-insulating SiC Substrates
SiC Epitaxy
N-Type & P-type Epitaxial Layers
Nitride Epitaxy
GaN, AlInN, InGaN Epitaxial Layers

View as InfographicOpen in New Tab/Window

Physical Properties

Polytype
Single-Crystal 4H
Supported diameters
150mm
Crystal structure
Hexagonal
Bandgap
3.26 eV
Thermal conductivity (n-type; 0.020 Ω*cm)
a~4.2 W/cm • K @ 298 K
c~3.7 W/cm • K @ 298 K
Thermal conductivity (HPSI)
a~4.9 W/cm • K @ 298 K
c~3.9 W/cm • K @ 298 K
Lattice parameters
a=3.073 Å
c=10.053 Å
Mohs hardness
9

Dimensional Properties, Terminology, & Methods

Diameter
The linear dimension across the surface of the wafer. Measurement is performed using an automated micrometer, traceable to the ANSI standard, providing the average value for each individual wafer.
Thickness, Center Point
Measured with ANSI-certified non-contact tools at the center of each individual wafer.
Surface Orientation
Denotes the orientation of the surface of a wafer with respect to a crystallographic plane within the lattice structure. In wafers cut intentionally “off orientation,” the direction of cut is parallel to the primary flat, away from the secondary flat. Measured with x-ray goniometer on a sample of one wafer per boule in the center of the wafer.
Orthogonal Misorientation
In wafers intentionally cut “off orientation,” the angle between the projection of the surface normal onto a (0001) plane and the nearest [1120] direction.

Materials Tools & Support

Materials Catalog

Knowledge Center

View All
Power
|
Air Conditioning

Design Next-Generation Data Center Cooling Systems with Silicon Carbide

Data center cooling systems account for 20-45% of power consumed by data centers. The efficiency of these cooling systems can be improved with silicon carbide leading to up to 50% reduction in system losses.
Continue Reading  Technical Articles

Footer

Social Media

  • Facebook
  • Instagram
  • X
  • LinkedIn
  • YouTube
Copyright © 2024 Wolfspeed, Inc.