Wolfspeed Talks 5G and Launches New Radar Technologies at European Microwave Week
MADRID, Sept. 24, 2018 – This week, the top players in the radio frequency (RF) technology and microwave components industry will discuss the latest innovations and trends at European Microwave Week. Wolfspeed, a leader in the RF power semiconductor market, is sharing their view on the upcoming 5G market while unveiling their expanded portfolio of radar and 4G/5G products.
Gerhard Wolf, vice president and general manager of Wolfspeed’s RF division, will deliver an industrial keynote on the technological challenges posed by the transition to 5G and how the industry can leverage GaN and LDMOS to achieve the greater bandwidth and efficiency that 5G requires. The company will also feature its new wideband, two-stage, LDMOS integrated power amplifier (PTNC210604MD) in a live demo at the event.
In addition to showcasing new communications parts, Wolfspeed will unveil two new radar parts: the CMPA5259025F – 25 W, 28 V GaN MMIC PA and the CMPA5259050F – 50 W, 28 V GaN MMIC PA. These C-Band MMIC Power Amplifiers are designed in a compact 0.5” square package with greater than 30 dB small signal and nominally 50% drain efficiency. This combination enables phased array radar designers to maximize the power per element for C-Band radar systems.
Both components are also used in linear and compressed amplifier circuits in marine radar, weather monitoring (Doppler weather radar), air traffic control (ATC), maritime vessel traffic control services (VTS), and port security applications. The 50 W MMIC PA for C-Band Radar enables modular system design with increased reliability and lower maintenance costs, making it applicable to a variety of emerging radar applications. For example, the new amplifier is an ideal solution for countries like India and USA as they upgrade radar capabilities at airports across their nations.
The CMPA5259025F – 25 W, 28 V MMIC PA and the CMPA5259050F – 50 W, 28 V MMIC PA are commercially available.
Cree® and Wolfspeed® are registered trademarks of Cree, Inc.
About Cree, Inc.:
Cree is an innovator of Wolfspeed® power and radio frequency (RF) semiconductors, lighting class LEDs and lighting products. Cree’s Wolfspeed product families include silicon carbide materials, power-switching devices and RF devices targeted for applications such as electric vehicles, fast charging, inverters, power supplies, telecom and military and aerospace. Cree’s LED product families include blue and green LED chips, high-brightness LEDs and lighting-class power LEDs targeted for indoor and outdoor lighting, video displays, transportation and electronic signs and signals. Cree’s LED lighting systems and lamps serve indoor and outdoor applications. Please refer to www.cree.com for additional product and Company information.