Mail Icon postage letter Location Marker standard map marker Pencil Icon pencil Power Icon Lightning Bolt Radio Frequency Icon Radio Tower Radio Frequency Icon antenna Search Icon magnifying glass Outgoing Call Phone with arrow pointing out Incoming Call Phone with arrow pointing in Next Arrows 2 forward facing arrows Down Arrow Downward pointing arrow Download File tray with arrow pointing in Pencil pencil Document document Info info Power circle icon lightning bolt with circle around it RF Components circle icon antenna with circle around it Wolfspeed circle icon wolfspeed logo with circle around it Wolfspeed wolf icon wolfspeed logo Marker Icon with Circle map marker with circle Page Icon with Circle page marker with circle Gear Icon with Circle gear marker with circle Page Icon with Circle page marker with circle Play Button Triangle on top of circle Large Right Arrow Circle Facebook Icon Twitter logo LinkedIn logo YouTube logo Right Arrow Right Arrow - thinner Handshake Icon Envelope Icon
Close

Thanks, we’re glad to hear from you.
We’ll route your inquiry to the proper division and they will respond promptly.

Close

Work with Us

BaSiCs of SiC Series: The Extreme Durability of Silicon Carbide

In the last blog, we looked at the basic properties and applications of SiC. In this blog, we look more closely at SiC’s durability and examine how important that durability is for its many different applications.

Silicon carbide (SiC) is a ceramic material that, for the purposes of semiconductor applications, is often grown as a single crystal. Its inherent material properties, combined with being grown as a single crystal, make it one of the most durable semiconductor materials on the market. This durability goes far beyond just its electrical performance.

Physical Durability
SiC’s physical durability is best demonstrated by looking at some of its applications outside of electronics: it is used in sandpaper, extrusion dies, bulletproof vest plates, high-performance brake disks, and flame igniters. SiC will leave scratches on an object rather than be scratched itself. When used in high-performance brake disks, its long-term wear resistance in harsh conditions is put to the test. To be used as a bulletproof vest plate, SiC needs high physical strength, as well as good impact strength.

SiC’s use in flame igniters shows that it can also withstand extreme temperatures. When temperatures reach around 2700°C, SiC sublimates directly to the vapor phase, meaning it becomes a gas. For context, the melting point of iron is around 1500°C, so in order for a SiC component to change phase, most of the metals around it would have already melted. SiC can continue to perform at temperatures that would destroy Silicon (Si).

Chemical and Electrical Durability
SiC is commonly known for its chemical inertness — it’s not attacked by even very aggressive chemicals like alkalis or molten salts, even when exposed to extreme temperatures of up to 800°C. As a result of its resistance to chemical attack, SiC is non-corrosive and can handle tough work environments that include exposure to humid air, saltwater, and a wide array of chemicals.

Because SiC has a high energy bandgap, it is extremely resistant to electromagnetic disturbances and the damaging effects of radiation. SiC can also handle higher levels of power without damage than Si.

Thermal Shock Resistance
The ability to withstand thermal shock is another key feature of SiC. Thermal shock occurs when an object is exposed to an extreme temperature gradient (i.e., when different sections of an object are at significantly different temperatures). As a result of this temperature gradient, the rate of expansion or contraction of those different sections will vary. In brittle materials, thermal shock can lead to fracture, but SiC is highly resistant to these effects. SiC’s thermal shock resistance is a combination of high thermal conductivity (350 W/m/K for a single crystal) and a low thermal expansion compared to most semiconductor materials.

SiC’s durability is one of the reasons why SiC electronics (e.g., MOSFETs and Schottky diodes) are being used for applications with aggressive environments such as HEV and EVs. Its physical, chemical, and electrical durability make it an excellent material for use in semiconductor applications requiring toughness and reliability.

Get in Touch
Work with us.